ECAT.MISSEDRXCOUNT
Description
This command can read the actual counter value of the SM2 event missed counter. This is checked against the limit set by the object 0x10F1 sub 2 (ECAT.MAXSYNCERROR). Fault F7011 is thrown if this counter reaches the limit and theEtherCAT communication state will change to SAFE-OP with an AL status code 0x34.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-04-000 |
General Information
|
Type |
ReadOnly |
|
Units |
N/A |
|
Range |
0 to 65532 |
|
Default Value |
9 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
EtherCAT variants: AKD2G-SPE